Model Configuration
Once an asset model is created, it can be associated with an equipment, so that the actual condition monitoring can begin. By configuring an asset, we mean associating an equipment with an available asset model, where the thresholds are decided for the rule-based models, or the AI ML models are trained with relevant data set.
Model Configuration module enables you to associate an equipment with an asset model created in Asset Model Library, which enables the condition monitoring of equipment.
To access the Asset Model configuration module of Predictive Maintenance Workplace application, go to Genix Platform > Digital App Center > My Apps > APM Model Configuration and Deployment > Model Configuration and Deployment. > Model Configuration module. The page provides a list of configured models, and it provides an option to configure a new equipment.
You can also click icon in the menu bar on the left of the Predictive Maintenance Workplace application from Asset Model Library and Predictive Maintenance Workplace modules. The Model Configuration home page is displayed.
Model Configuration Home Page
Model Configuration Workflow